Part Number: LMX2594EVM
Other Parts Discussed in Thread: LMX2594
I am using the LMX2594 to output a SysRef signal through TICs Pro. I have successfully output my desired clock signal through output A, but the SysRef signal is not showing on a spectrum analyzer.
I followed the user guide step-by-step with no success. I set VCO_PHASE_SYNC, SYSREF_EN, SysRefReq to high, while changing the appropriate PLL parameters and powering up output B's mux. I am outputting the SysRef signal single-ended with a termination on the unused port.
I am unsure of several steps in the process:
- User guide and data sheet require that I put the board into SYNC mode (category 1). To do this, I simply set VCO_PHASE_SYNC = 1 and follow the instructions for IN_PIN_IGNORE. (I have tried this both with and without a 10 MHz SYNC input but no success.)
- Data sheets says to "Apply the SYNC." It does not give specific instructions on how to do this. I toggled the SYNC pin but it also did not work.
- I am using output B's mux to output the SysRef signal; however, there is a SYSREF port on the LMX2594, which I leave unused but am weary.
Are there any additional steps needed to output the SysRef signal that are not explicitly stated on the user guide/data sheet?