Part Number: LMX2571
Other Parts Discussed in Thread: ADS6125
I'm not able to find out how calculate the output frequency from SNAS654A.
Suppose
OSCin=26MHz
Output frequency=20MHz
The synthesizer mode is selected.
Set the value of the output channel divider of R22 register.
Is the VOC frequency divided? If it is . VOC frequency is from 4300 to 5376 MHz. How to determine the VOC frequency.