Part Number: LMK04828
Other Parts Discussed in Thread: ADC32RF45, , LMK04610, LMX2582, LMK01010
I'm investigating a lower power clocking solution for an ADC32RF45 based receiver design. I posted questions on the High Speed Forum related to this:

The concern is that the ADC32RF45 EVM uses the LMK04828 to generate SYSREF for the ADC as well as the EVM FPGA, as well as the FPGA clock. The data sheet for the LMK04828 indicates power dissipation of 1.9W.
Is this power dissipation accurate if the device only outputs SYSREF signals, or is there another, simpler clocking device that could be used instead of the LMK04828?