This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Clock Generation Recommendation

Other Parts Discussed in Thread: LMK61E0M, CDCEL913

Hi Team,

Could you help to recommend a clock generation device that can meet below spec? It is used for Notebook GPU clock input.

• Frequency: 100 MHz.

• Voltage swing: 1.8 V.

• VIH = 1.45 V (min)

• VIL = 0.45 V (max)

• Accuracy: ± 10 ppm at room temperature, (± 30 ppm overall (including temperature drift)).

• Duty cycle (worst case): 45-55 (max).

• 200 ps (max) cycle-to-cycle jitter.

• 300 ps (max) long-term jitter (10,000 cycles after the triggered edge).

Thanks,

Nic