Part Number: CDCE72010
Other Parts Discussed in Thread: ADS5562EVM,
Hi,
I currently have a 200MHz XO mounted on the ADS5562EVM. I made modifications to the EVM board to accommodate the XO (original design calls for a VCXO). What I'm expecting is to see a 50MHz signal coming out from the U1N output since TI factory programmed it with divide by 4. However, I'm not seeing any signals at the moment but I've also noticed that the CDCE72010 is incredibly hot (+50 degrees cel. ambient). I've also set all the appropriate jumpers to enable the CDCE chip on the ADS5562EVM.
Ron.