Other Parts Discussed in Thread: LMK03328, LMK03318, USB2ANY, CDCM6208
Hi,
We are looking for a clock synthesizer of following specs:
1. Pre Programmed using TI Programmer Jig and Software
2. Min 8 to 10 nos of LVDS Clock outputs until 700MHz
3. Re programming of Output values using I2C or SPI Interfaces
4. Dual Input options
We had used a Silicon Lab's part SI5338N-B-GM in couple of designs. It is a 4 output clock synthesizer which can be one time pre-programmable using their own application + it can also be re programmed through SPI Interface. We want similar device with 8 to 10 outputs. Please suggest if you have any recommendations.
Regards,
Vijetha