This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK04828: PHASE NOISE VALUES FOR LMK04828

Part Number: LMK04828

Dear sir,

We are using LMK04828 Dual PLL in our design. For this we required phase noise values for various frequencies as mentioned below,

Input Frequency to PLL : 25MHz (SiT5000AI-8C-33E0-25.000000)

VCXO Frequency  : 100MHz(CVHD-950X-100.000)

Output frequencies :

DCLKOUT0 : 120MHz , LVDS mode , provide for 60MHz also

DCLKOUT2 : 240MHz , LVDS mode

DCLKOUT4 : 100MHz , LVDS mode

DCLKOUT6 : 100MHz , LVDS mode

DCLKOUT8 : 2400MHz , LVPECL mode

DCLKOUT10 : 100MHz , LVDS mode

SDCLKOUT5 : 100MHz , LVDS mode

SDCLKOUT9 : 10MHz , LVDS mode

SDCLKOUT11 : 10MHz , LVDS mode

Regards,

Jaya Bharath