Part Number: NE555
Other Parts Discussed in Thread: LMC555, TLC555,
Hello,
I have selected NE555PSR for my project from TI. Basically application to generate 12V ,90 KHz frequency output with duty cycle 81.21.
To achieve the above condition I have used Ra=10K (1% tolerance), Rb=3.01K (1% tolerance) and C1= 1nF(5% tolerance).
As per theoretical calculation the output value is 90.075 KHz and duty cycle 81.21 with the said components value. But in real time in the circuit practically while I was verifying I got output frequency approx 65 KHz. and duty cycle approx 81.
I am not understanding, why there is this much deviation of frequency output from theoretical value to practical values??
Kindly suggest me how can i achieve the expected output frequency.
Thanks in advance.
DEBPRASAD