Part Number: LMX2571
Hi Team
I'm using PLLatinum Sim to find the lock time for phase and freq error - 1deg and 1kHz
The model included VCO cal time and analog loop dynamic time.
However, for the frequency switching I want to do, will involve changing the output dividers.
Assuming we write these registers in the fastest time possible allowable by the lmx2571, can you tell me how fast the dividers switch and settle.
Example cases:
Fstart Fstop
10MHz 1344MHz
500MHz 501MHz
1000MHz 1100MHz
500MHz 1000MHz
Regards