Hi,
we're planning to use the TI CDCE62005 in a new project and want to generate a variety of clocks which in the end need odd output divider settings (e.g. 5).
In the datasheet, the duty cycle of the output is between 45% and 55%, without giving a clue whether a special divider setting is used here.
Does this duty cycle also apply to odd divider settings like 3 or 5 or will these settings modify the duty cycle? (like in competitors solutions)
Regards,
Jan