Part Number: LMX2594
Dear Team,
My customer considers the LMX2594 for a very wideband design covering from 2GHz-15GHz.
The harmonic at low frequencies are very strong. They have measured 3rd harmonic of -12dBc with f_out=2GHz.
1. Is this indeed what they should expect ?
2. Is there any trick we can use to reduce the 2nd and 3rd harmonics at low frequencies ?
3. Is there any change on the harmonic performance if they use it without the output dividers ? (VCO only on the output)
4. Any additional tip or trick you would be appreciated.
Best regards,
Nir.