Part Number: CDCE72010
I am using this IC in a new design.
The IC outputs clocks properly, freq, etc .... but it doesn't power up well.
Being powered off from an infinite amount of time, once powered up, the device is lasting to output a clocks about 30 or 40 seconds.
Once this happen, if powered off and powered up again, it outputs clocks almost instantaneously.
The values of the registers I am writing to the EEPROM are:
REG0 = 0x682C0230
REG1 = 0x68840241
REG2 = 0x68840002
REG3 = 0x688402A3
REG4 = 0x68840004
REG5 = 0x680C00A5
REG6 = 0xE9040006
REG7 = 0x21840317
REG8 = 0x210C0078
REG9 = 0x69400059
REG10 = 0x0EA41D4A
REG11 = 0x0000089B
REG12 = 0x0000180C
The VCXO is 600 MHz, and the loop filter is C1=100nF, C2/R2 = 22uF/7K, R3=1K and C4=100nF.
Digital control lines, PD and RESET are OK, and the device is in SPI mode.
Could you help me with this problem?
Thank you in advance!
Jose