This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2594EVM: How to generate "1900.67MHZ " signal

Part Number: LMX2594EVM


HI,

I want to generate 1900.067MHZ signal from the LMX2594EVM. Can any one suggest me the possible combination in "TICS Pro software".

FYI......

Noted Thank you.

  • Dear Sing,

    thank you for reaching out. The EVM come with multiple option for reference. If you use the 100 MHz reference on the EVM pcb directly, you can simply type 1900.67 on the output box of the TiCS PRO software and all setting will be calculated for you. The software will pick a output divider by 6 but may also use a divide by 4.

    oscin=100
    R=1
    pfd=100
    N=76
    num=67
    den=2500
    vco=7602.68
    D=4
    out=1900.67

    with divide by 6 (D):

    oscin=100
    R=1
    pfd=100
    N=114
    num=201
    den=5000
    vco=11404.02
    D=6
    out=1900.67

    Hope this helps,

    Regards, Simon.
  • Hi Simon,
    This is ayyappa.
    I gave wrong value 1900.67MHZ to you. Actual our point of interest is 1900.067MHZ.Could you please give me the configuration for this?

    Thank you
    Ayyappa