Hello,
I am operating the LMX2594EVM with a Fpd of 20 MHz. I have the N divider set to 376 and am using the 7.52 GHz directly from the VCO as the output. I am measuring -70 dBc spurs at 10 and 20 MHz offset. Is this an expected result under these conditions?
Reducing the charge pump current (reducing the PLL bandwidth) improves spur performance. However, the minimum (and best performing) value I can choose using the TICS GUI is 3 mA. There is an option for 0 mA, but the PLL loses its lock at this setting. I would like to continue lowering the charge pump current to hopefully continue lowering the spurs. Is there a way to set the charge pump current to a custom value less than 3 mA?
Thanks
Alex