Part Number: CDCEL9XXPROGEVM
Other Parts Discussed in Thread: CLOCKPRO, , CDCE913
I have just got my new CDC Programming EVM in order to program a CDCE913. I have severe problems in installing the software in a proper way. In the User Manual is said that there shall be an accompanying CD. There is no CD in the package.
The manual suggest those steps:
1. Connect the EVM with the PC with a 2.0 USB cable. OK so far.
2. Install the driver software using the provided CD-ROM. No CD or drivers found
3. The EVM is now running and completely powered through USB. The LED’s D2 (3.3 V) and D3 (1.8 V)
indicate the availability of the supply voltages. CHECK..
4. I used the ClockPro for program.
5. My operate system is Win7 Pro.
6. only show the disconnect (dark green )
7.some time could show like this ,but can not progam ,the program button always grey.
Could some one help me to solve this problem?
Thanks
Fei