Part Number: LMX2571EVM
Other Parts Discussed in Thread: LMX2571, CODELOADER
Hello,
I want to generate two cycles frequency with LMX2571 EVM, 235MHz and 280MHz. Register values are configured by default, then alternant switch register R0 to achieve frequency switching in BurstMode of CodeLoader 4. The Switching Period is 30ms, and both frequencies are correct.
However, there is a lot of spurious near the center frequency. The spectrum of two frequencies is shown in the figures.
Why the spurious frequency is so much.