Part Number: LMX2594EVM
Other Parts Discussed in Thread: LMX2594
Hi,
I'm working on a research project which requires two signals (up to 13 GHz) generated from a function generator and they need to be synchronized in phase with the potential to change the phase for each independently. I checked the mentioned kit and I think it would meet my requirement. What do you think?
If yes, I noticed that the power supply cable is connected via an SMA connector. Is there any special specification for this power supply?
Thanks,