This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2595EVM: LMX2595 300Hz side tones

Part Number: LMX2595EVM
Other Parts Discussed in Thread: LMX2595

The LMX2595 shows  250-300Hz side tones of significant magnitude on either side of the carrier.  These are not present in the clock ref provided to LMX2595.  This was measured on the LMX2595 eval board.  Is there a way to get rid of these? where are they coming from?  again this was the eval board without mods. 

We also see a lot of bleed through of what appears to be the ref clock also at offset of the ref clock over a side range,  these are typically at 50-60dBc down but still kind of annoying.  Is there way to improve this?

Images attached both spectrum and phase noise plot  of the 300Hz issue

Thanks,

Steve