Part Number: LMK61PD0A2
Other Parts Discussed in Thread: LMX2572
I have an LMX2572 eval board that came with the reference PRO board. The reference PRO (LMK61PD0A2) is supposed to be able to provide different clock freqs such as 62.5MHz, 100MHz, 106.25MHz,.. My first question is can these frequencies be controlled by software? or the only way is to strap the FS1 and FS0 jumpers to appropriate pin? Also, when I change the FS1 and FS0 configuration according to the datasheet, I still get only 100MHz as output. Am I missing something? Thank you in advance!