I've recently received the CDCE706 evaluation module. I'm using a 50 Ohm SMA cable to connect an output to a high bandwidth (4 GHz) scope (on a 1 M Ohm input); I've connected 3.3V supplies to all three supply rails. I get the correct frequency out, but with 20% jitter on the period. I've programmed the module using the supplied software and parallel interface (to try out different frequencies, and to see what happens if I bypass the PLLs): the frequency changes as intended, but I can't get rid of the jitter. Am I doing something wrong, or is there more likely a problem with the on-board crystal oscillator?