This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK04832: CLKSEL0 & CLKSEL1 used for readback

Part Number: LMK04832

Hello,

I see that the CLKSEL0 & CLKSEL1 pins can be programmed to be used for readback outputs.

I do not fully understand what is possible to be read back...

1. If used for readback, do they replace the SDIO pin for readback function?

2.Is there any information that can be read back from teh CLKSEL0 & CLKSEL1 pins that cannot be read from the SDIO pin?

Regards,

Itai