Hi, I want to use TCXO as a reference clock for my LMK00304. However, I can not be sure about TCXO's driving capabilities and how to use it with LMK00304. TCXO has a LVCMOS output(High Voltage = 3V, 100MHz) with 4ns rise/fall time and +-4mA current. How can I use with LMK00304, should I connect TCXO's output directly to the LMK CLKin ? TCXO has 15pF capacitive output, and I guess LMK00304 has high impedance input right ?
Also according to the these informations TCXO's slew rate is far below 3V/ns(LMK00304 test conditions). So How much degradation of performance should I expect from my LMK00304?