Part Number: LMX2592
Hi,
I would like to know if it is possible to use a DDS wth for example 50 MHz to 90 MHz as reference frequency to generate 5 GHz - 9 GHz.
While sweeping the DDS per Software command step by step, is it possible to operate LMX2592 without calibration? Just by knowing the VCO core and switching accordingly? I there also a switching VCO tuning capacitors involved in the calibration process? What would be the lowest switching delay method to implement such a sweep?
with kind regards,
Gerhard.