Part Number: LMK61E2
Other Parts Discussed in Thread: LMK00304, LMK03806,
Hello
in my design I have a ZYNQ FPGA board. it can produce a clock signal base on the PLL-block. but I think the jitter is not low! so I can not use it to feed the high speed ADC/DAC.
I'm looking for a solution to keep the datasheet's spec and minimize the price/ pcb design/time...
I can have some plans as follow:
generating a clock using FPGA----->clock driver-----> 200MHz for the 14-Bit DAC (LVDS or CMOS)
------> 65MHz or 80MHz for the 14-Bit ADC (LDVS or CMOS)
using for example LMK61E2---> clock driver---> ADC/DAC/ plus to the FPGA bcoz I should synq the DAC with FPGA
using for example LMK61E2---> ADC/DAC/ plus to the FPGA bcoz I should synq the DAC with FPGA
or other plans...
Do you have any suggestions? I need a certain and reliable solution.
Best Regards