This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2582: LMX2582 1.8V IO support

Part Number: LMX2582

Hi, Experts:

We are trying to interface with LMX2582 with 1.8V IO due to the limited resource of 3.3V IO in FPGA.

For the digital input signal of LMX2582, I think we need to make sure the  MIN number of VOH of FPGA >1.4V and MAX number of VOL< 0.4V.

For the digital output signal of LMX2582, I can use a resistor divider like 10K series resistor and 12K shunt resistor to divide the 3.3V IO down to 1.8V, and also check the input spec of FPGA.

 Can you please help to double check if you see any issues regarding this?

Thank you so much for your promot help!

Yarn,