Part Number: CDCE913
Other Parts Discussed in Thread: CDCLVC1103
Hi,
I have an application where I need to drive 3 20 bit sigma delta ADC's with a clock. I was originally using a CMOS oscillator with a 45% - 55% duty cycle specification thru a CDCLVC1103 buffer. The concern was that running through the buffer would further degrade the duty cycle specification. I was then looking at the CDCE913 as an option as per the datasheet it does not seem to have duty cycle degradation. The desire was to run it in PLL bypass mode, but there does not seem to be any information on if running in bypass mode has any effect on the specifications. Can you advise if the CDCE913 is a better way to go, or is there another product that would work better?