Part Number: LMX2594
Other Parts Discussed in Thread: LMX2592
Hello
Can input clock signal be applied to he LMX2594 input before it is powered?
Regards,
Itai
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Noel,
Which electrical specifications?
The ones that states in the "electrical characteristics" that Vin should be between 0.2Vpp-2Vpp?
or
The ones in the LMX2592 datasheet under "absolute maximun ratings" that states that when Vcc=0V Vin should not pass 1Vpp?
Please clarify.
Regards,
Itai
I appologize for nagging about it :), but the LMX2594 datasheet does not refer to the condition where the device is unpowered (Vcc=0V).
The only reference to the OSCin input voltage range is under the electrical characteristics section (Vcc=3.3V) where it is stated that the input voltage may be in the range of 0.2Vpp-2Vpp.
Can I apply 0.2Vpp-2Vpp when Vcc=0V?
Regards,
Itai