Hello,
Regarding to current consumption on CDCLVD2102, my customer is asking a question.
They use only two inputs(INP0/INN0) and remain inputs are connected to pulldown..
INP1/INN1:1K ohm pulldown
OUT2/OUT3:OPEN
(Question)
How many supply current does it consume at using two inputs(INP0/INN0)?
(According to datasheet, the supply current is 106mA(max) at using all input ,800MHz.)
Regards,
Tao2199