Part Number: LMX2594
Hi,
I am planning to use LMX2594 in one of my designs. In the datasheet, typical characteristic graphs are given with various output jitter values.
- I would like to know what should be the input reference clock spec to meet these jitter values.
- Will the jitter response be affected by input reference clock frequency also.
I am planning to use an input reference clock of around 1GHz to get an output ranging from 10GHz to 15GHz. It is very critical for me to achieve the output jitter values similar to what is mentioned in the datasheet.