Hi,
In the Eval board schematics, If VccVCO, VccBUF, VccPLL, VccDIG are of same voltage, can i connect all these via single resistor and capacitor instead of multiple resistors & capacitors of same value?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
In the Eval board schematics, If VccVCO, VccBUF, VccPLL, VccDIG are of same voltage, can i connect all these via single resistor and capacitor instead of multiple resistors & capacitors of same value?
Hi Lane,
We have below doubts:
1. If we are using single supply, what shall be the values of R2 & C2? Will there be any change in specifications or working if we go with the single supply configuration?
2. In eval board BOM, C2,C3,C4,C5 are made open. If so how does the resistor R2,R3,R4,R5 helps in filtering?
3. Also bypass capacitors C9,C17,C18 are also made open.
Sachin,
Yes, this is a good approach.
For testing purposes with our EVM, put 0 ohm resistors for the ones that you plan to leave out in your design.
Regards,l
Dean