Part Number: LMX2581
Dear,
i'm using the LMX2581 product and emulating in my application board.
i'm trying PLL 150MHz locking with reference clock 20MHz and using the internal VCOfor.
reference clock 20MHz
output : 150MHz
but locking was failed.
Could you check the setting value. my resister setting is below.
R5 (INIT) 0x40870010
R15 0x021FE7BF
R13 0xF082C10D
R10 0x210050CA
R9 0x03C7C039
R8 0x207DDBF8
R7 0x1C082307
R6 0x000004C6
R5 0x00012805
R4 0x00060004
R3 0x2019E543
R2 0x04000002
R1 0xC00020A1
R0 0x441A0000