This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK04208: Phase Noise Issue in Signle PLL Mode with PLL2 only, and Need Reference Configuration

Part Number: LMK04208

Hi, Team

My telecom customer is using LMK04208 in their MDAS project. They use signle PLL mode with PLL2 only. The spec is below:

Input: 25MHz single-ended with 0.4Vpp to OSCin.

Output: CLKout0&1&2&5 = 156.25MHz (LVDS), CLKout3&4 = 20MHz (LVCMOS single-ended, use OSCin frequency directly).

Loop filter configuration:

Customer find the phase noise of CLKout is big.

Could you share a reference configuration according to customer's spec?

Thanks

Kevin Zhang