This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK03328: I can’t program the EEPROM

Part Number: LMK03328

Hello,
I can’t program the EEPROM in LMK03328 device.
Using codeloader4 ver4.20.2, partfile ver1.0.0
I follow the EEPROM Programming Flow in SNAU185 document.
Reg. value write is okay but EEPROM program is failed.
The device and configuration information are below,
VNDRID : 4107
PROID : 50
REVID : 1
PRTID[31:24] : 1
PRTID[23:16] : 0
PRTID[15:8] : 218
PRTID : 152
HW_SW_CTRL_MODE : EEPROM MODE
GPIO32_SW_MODE : LL
HW_DFLT_MODE : EEPROM/ROM Mode
OP_MODE : EEPROM Mode
GPIO_HW_MODE : 0
SLAVEADR_GPIO1_SW : 85
EEREV : 0
Thanks for your help.