Part Number: CDCV304
Hello,
My customer has a question about maximum value of "Additive phase jitter from input to output 1Y0".
So could you please comment on the questions below?
[Q1]
Could you tell me the maximum value?
Or, do you have any comments on the maximum value
For example, comments like "Maximum value is not more than twice the typical value" .
[Q2]
Their specifications are as follow.
・Input RMS Jitter (max) = 1psec
・Required Output RMS Jitter (max) = 2.5psec
Could you try CDCV304 Output RMS Jitter estimation by using their Input RMS Jitter data?
Can CDCV304 satisfy their requirement?
[Q3]
In order to satisfy their requirement, Additive Jitter must be less than 2.29psec.
Jadd = √ (Jttotal^2 - jsource^2) = √ (2.5psec^2 - 1psec^2) = 2.29psec.
Is there a possibility that the maximum value of Additive Jitter of CDCV304 will be larger than 2.29 psec?
Best regards,
Kaede Kudo