Other Parts Discussed in Thread: TLC555
Hello guys,
One of our customers wants to use NE555 as VCO(Voltage-controlled oscillator).
Could you please give me any schematic if you have?
Your reply would be much appreciated.
Best regards,
Kazuya Nakai.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Kazuya,
This circuit should work from 0 to 3 kHz as pin 5 goes from 5V down to 0.5V (VCC = 5V)
I simulated this with similar TLC555 model which doesn't output correctly for pin 5 near 5V. However, in real device I don't believe that will be the case for NE555 (or even TLC555). I might be able to test this circuit next week.