This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PLLatinum Sim 1.5 rev F issue



I used PLLatinum Sim to estimate filter parameters for 60 Hz operation. I understand that the tool, most likely, has not been intended for such low frequency simulation, but it actually performed OK until that last version (1.5_F). The issue is that I can no longer input value 0.00060 MHz in the VCO field - any value below 0.001 MHz is automatically reset to 1000 MHz (screenshot of the previous version is attached). Can this issue be addressed in next version? How can I download the previous version?

Sincerely