I intend to configure the registers in the CDCE62005 device to generate 76.8MHz clock (with auxillary being connected to 38.4MHz crystal) and also get a synthesized 40MHz AND 80MHz outputs (from 80MHz oscillator connected to the primary).
As it is, I'm using one internal VCO for generating 76.8MHz (LVDS) and using 80MHz oscillator, i'm deriving 80MHz (LVDS) and 40MHz (LVDS) outputs.
I wanted to know if other frequencies like 66MHz or so on can be derived simultaneously by using another VCO.
Request help!!!
Vinay