Part Number: LMK04828
Other Parts Discussed in Thread: LMK04832
Hi,
I have PLL2 VCO output of 3GHz that I intend to use as device clock to my adc on the same board with LMK04828. Thus I need this signal to directly go through DCLKoutX_MUX. I can do this by setting DCLKoutX_MUX=2 which is the bypass mode, however since I skip the divider by choosing bypass mode do I lose synchronization between sysref and DCLKout since I skip the divider?
I can also try setting divider=1 to make sure that DCLKout goes through the divider and syncronized by sysref, however If I choose divider=1 I can't set DCLKoutX_MUX=0.
Erdal