This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65LVDS105: using 2 LVDS Repeaters to have 8 outputs

Part Number: SN65LVDS105

Dear,

I want to use 2 SN65LVDS105 LVDS Repeaters to have 8 similar outputs to serve for a fixed 50 MHz LVDS compatible clock signal.

My clock signal is generated by a MiniZed board. The output of the MiniZed is 3.3 V.

My question is can I connect the output of the MiniZed directly to 2 inputs SN65LVDS105 LVDS Repeaters or do I need some translation or resistors to distribute the signal?