I am working on a design in which we would prefer not to include a crystal, but only a 16 MHz single ended LVCMOS reference clock.
Is it possible to program the device ahead for this option, then use it on a board which does not have a crystal input?
A related question - is there any way to program the device without first providing a 25 MHz crystal input? From the datasheet it is not clear which input clocks the SPI interface, but I am assuming it comes out of the smart multiplexer?
Thanks!
Rob