Part Number: CDCE62002
Hi ,
I'm trying to configure cdce62002, which have 148.5Mhz as input and generate output of 150Mhz.
following are the parameters:
REGISTERS
0 12B60050
1 B799E401
2 00000002
PORTS
0 DD
1 FF
2 DF
3 F9
INPUTS
PRI 148.50
AUX 0
EXTERNAL COMPONENTS
C4 6.8n
R4 2k
C5 180p
SPI write/read are verified.
My problem is PLL is not locking. Is the issue with parameters? or can anyone suggest any test case.
Thank-You in advance.