Other Parts Discussed in Thread: LMK03318
Hello,
I am using the LMK00105 with the following settings:
VDD = 3.3V, VDDOA = 3.3V, VDDOB=1.8V
Input signal: AC coupled LVDS driven by the LMK03318 device.
I did not understand whether I need to add external biasing after the AC coupling capacitors or not.
Right now I only added a 100 Ohm termination resistor at destination point.
Thank you,
Svetlana