Other Parts Discussed in Thread: TPL5000,
Support Path: /Product/Development and troubleshooting/
It would be REALLY nice if TI put out a spreadsheet or other calculator for this product. Even better would be a simple table of the values Rext = this time...
I have gone through the calculations and am pretty baffled by the quantization as it seems to indicate massive (+/- 6 second) steps in the setting 3 zone (10 - 100 seconds).
IN MY APPLICATION: I am using a 13.0K 0.1% accurate resistor, I was expecting a 15.0 second timing pulse, but instead I am getting 15.5 seconds.
Where did I go wrong?
T | 15 | Seconds | |
a | b | c | |
Use | 0.1972 | -19.345 | 692.1201 |
Rext | 13000 | Ohms | |
Rd | 130 | ||
Tadc | 6 | Seconds | |
Err | 60 | % |