Part Number: CDCLVC1110
Hello support team,
I have a question regarding CDCLVC11xx.
- Can CDCLVC11xx drive a CMOS IC (Vcc = 3.3 V) whose input capacitance is 20 pF with 50 MHz clock signal?
The period of 50 MHz clock signal is 20 ns. So I think the minimum current required to drive will be 20 pF * 3.3 V / (20 ns / 2) = 6.6 mA.
And I think that the power consumption will be about 47 mW by referring to the electrical characteristics and the footnote (3) of the data sheet on page 6.
Therefore, I guess the driving capability of CDCLVC 11xx is not problem.
Is my understanding correct?
Best regards,