Hello,
We're currently in the process of evaluating options for a design where we need to generate a clean, low-jitter square wave to feed a 100 Msample/sec A/D converter from a clipped-sine wave TCXO. I recently came across the CDC3RL02 sine-to-square wave converter chip, and this appears to be an ideal solution. Couple of questions here:
1) Is there an eval board for this part available?
2) All of the examples of the datasheet show a 1.8 Vpp sine wave coming in, and a 1.8 Vpp LVCMOS signal coming out. I'd like to confirm that, as the spec section indicates, if we feed it a 0.8 Vpp clipped sine wave input, that we'll get a 1.8 Vpp LVCMOS output.
3) The additive jitter spec defined in the datasheet is 0.41 pS RMS. Can I assume that this applies regardless of input type (clipped sine, sine, or LVCMOS)? We're obviously sensitive to any additional jitter, as it affects our overall SNR in the A/D converter.
4) The datasheet specs a minimum input signal swing of 0.3 Vpp. Are there jitter/phase noise specs available for lower voltage swing values such as this?
5) We don't need the LDO included in the chip, but it will be enabled whenever we enable either of the clock outputs. Is there anything we need to do on this output line to make it happy/stable if we aren't using it?
Thanks much for any feedback you can provide for the above.
Regards,
John