Part Number: LMK04616
Hi all.
I have some question about LMK04616, so please help me.
1. What are C4, R4 at PLL2? For 4rd Filter? I could not find the explanation in datasheet.
2. Register 0xAF and 0xB0, I want to know enable status.
Which is bit that PLL2_RDIV_CLKEN is enable, 0 or 1? I think enable bit is 1
Which is bit that PLL2_NDIV_CLKEN is enable, 0 or 1? I think enable bit is 0
3. Please tell me the setting range of PLL2_LD_WNDW_SIZE and PLL2_LD_WNDW_SIZE_INITIAL?
I can't understand the 0x85 and 0x86 register, Is 0x01 setting 2ns? If we write 0x3F, can we set 62ns?
Please tell me the relationship of register and windows size.
4. Please tell me the difference of Soft reset and SWRST. What is SWRST?
Sorry for many question, but I would like to get your comment as soon as possible.
Best Regards,
Sho