Other Parts Discussed in Thread: ADC12J4000EVM, DAC38RF82EVM, , TRF3765, DAC38RF82, ADC12J4000, ADC32RF45, LMK04828
Hi everyone,
We have bought two ADC12J4000EVM boards and a DAC38RF82EVM board. I'm wondering if TRF3765EVM is suitable to be a clock source for the ADC/DACs we have.
In my design, the two ADCs operate at a sampling rate of 3GSPS and the DAC operates at 3GSPS in dual channel mode.
Each ADC12J4000EVM requires two external clocks input, which are LMKCLK and DEVCLK. The DAC38RF82EVM also needs an external clock if my understanding is correct. So overall the converters need 5 clock inputs.
We're considering to buy a TRF3765EVM to serve as the clock source, but I'm not sure if this one is a good choice. Can anyone tell me if TRF3765EVM meets the requirements (such as signal quality, power level)?
Thank you.
Regards,
Tong