Part Number: CDCI6214
Hi,
I'm trying to make the CDCI6214 work, but still unsuccessfully. You might give me a useful advice...
The attached schematics is my actual circuit. I'm not expecting it to be wrong.
Regarding the software, I'm not sure about the configuration procedure. Following are the configuration of registers that are written to I2C Slave addres: 0xEC
FIrst, the voltage configuration of outputs is set, then all registers in order from 0x44 to 0x00 are written.
My problem is that I can control most of the functions, but the PLL won't lock an I also can't control outputs Y1-Y4.
I'm able to bring the reference clock only to output Y0, not to other outputs.
What is strange is that i have to apply RESET multiple times until the device responds to I2C commands.
Many thanks for your comments!
Stan
00280000
002E0000
00340000
003A0000
00440000
00430020
00420000
00410F34
0040000D
003F0210
003E4209
003D1540
003C0018
003B106B
003A0000
00390A65
00380405
00370012
00360000
00358000
00340000
00330A65
00320415
0031C005
003001EE
002FBA34
002E0000
002D0A65
002C0415
002BC00C
002A00DB
002986DB
00280000
00270A65
00260405
00250012
00240000
00238000
00220050
00210007
00200000
001F1E72
001E5145
001D421C
001C0000
001B3419
001A0718
00190000
00180001
00170000
00160000
00150000
00140000
00130000
00120000
001126C4
0010921F
000FA037
000E0000
000D0000
000C0000
000B0000
000A0000
00090000
00080000
00070000
00060000
00050020
00040041
00039000
000200D0
00016B82
00003000