Part Number: LMK05028EVM
Other Parts Discussed in Thread: LMK05028
Dear Sir,
I obtained TI LMK05028 EVA board and tried to operate with PC, function generator, frequency counter.
But I found one problem ‘ D12/D13, D8,D9 LED are still ON even I connected 2.048MHz CMOS to one of IN0,IN1, IN2,IN3.
USB connection (PC to Board) was confirmed on the software.
Please advise following 3 points.
Q1 How can I turn off LED D12/D13, D8/D9 ? Page1
Q2 I want to use external TCXO,OCXO. How are Jumpers set ? Page2
Q3 Pleasee advise the circuit connection. Page3
Kind Regards,