Part Number: LMK03328
Hi Team,
We have questions about R12 register from customer using LMK03328.
Could you please elaborate the following descriptions for each R12.2, R12.1, R12.0 ?
Q1). R12.2 : What is "always on clock" ? If set to "1" does it mean the output clock is not locked to input clock ?
Q2). R12.1 : What is the difference from the two settings ?
Does it mean VCO Calibration PLL1 and PLL2 run ...
"1" : simultaneously (PLL1 and PLL2 at the same time)
"0" : sequential ( PLL1, then PLL2)
Q3). R12.0 : I am understanding that this bit must be "1" to operate normal for the device. When do you use R12.0 = "0" ?
Best Regards,
Kawai